DUG_LK FUGA Wiser wireless dimmer_WH-00

Away Mode

Away Mode allows you to automatically turn off the dimmer when you are away from home for a longer period. The device stays off until you turn off Away Mode, helping save energy and prevent unnecessary lighting.

  1. On the Home screen, tap > Away Mode.

  2. Under the LIGHTS section, tap the Dimmer (A) toggle to add it in Away Mode.

  3. On the Home screen, turn on the Away Mode toggle.

    TIP: For more information on Away Mode, refer to Away Mode in the respective System User Guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.