DUG_LK FUGA Wiser wireless dimmer_WH-00

Technical Data

Nominal power

Load type

Load name

Load value

LED

1–130 VA

1–30 VA

Incandescent lamp

1–250 W

Halogen lamp

1–230 W

Iron core transformer

1–70 VA

Electronic step-down converter

1–200 VA

Nominal voltage

AC 230 V ~, 50 Hz

Standby

Maximum 0.4 W

Connecting terminals

Screwless terminals

2x 1.5 mm² (N)

2x 1.5 mm² (L)

1x 1.5 mm² (Load)

Ambient temperature

5 ... 25 °C

(temporarily up to 35 °C)

External fuse protection

16 A circuit breaker

Operating frequency

2405 ... 2480 MHz

Max. radio-frequency power transmitted

< 10 mW

Communication protocol

Zigbee 3.0 certified

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?