DUG_LK FUGA Wiser wireless dimmer_WH-00

Assigning a moment to the push buttons

A moment allows you to group multiple actions that are usually done together. You can configure a moment to the push buttons, such as Good Night Moment: light dimming 50%, shutter close.
  1. On the Control tab, tap All devices or the room tab where the dimmer is located.
  2. Tap > Configure buttons.
  3. Tap any key and select Moment.
  4. Select an existing Moment which you want to add to the key and tap Select Moment.
    TIP: To create a new moment, refer to Creating a Moment in the respective System User Guide.

    In the next screen, shows the Moment is successfully configured.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.