DUG_LK FUGA Wiser wireless dimmer_WH-00

Adjusting the brightness level using app

  1. On the Control tab, tap All devices or the room tab where the dimmer is located.
  2. On the Device Control Screen, drag the slider bar up/down to increase/decrease the brightness (A).
    TIP: Tap (B) on the Device Control Screen to turn the dimmer on/off.

    NOTE: When the power button (B) is turned off, the brightness slider is disabled. To adjust the brightness, first turn on the power button, then move the slider to your desired level.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.