DUG_LK FUGA Wiser wireless dimmer_WH-00

Setting up the Dimming Mode

Dimming Mode allows you to configure how the dimmer operates based on the type of connected lighting load. This feature helps optimize performance and prevent issues such as flickering or overheating.
  1. On the Home screen, tap .

  2. Tap Devices > Lights.

  3. Select the dimmer and then tap LED Indicator Behaviour.

    NOTE: If you are unable to find this option in your app, reset the device to factory default and perform the pairing process.
  4. Select one of the following options as per your preference, and then tap Done.

    • RC Mode: Use when different load types are connected to the dimmer.

    • RL-LED Mode: Use to improve dimming quality if you have problems with light flickering. Recommended when LED lights flicker or behave inconsistently in RC mode.

    NOTE: RC Mode is selected by default.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.