DUG_LK FUGA Wiser wireless dimmer_WH-00

Using the device

The Device Control Screen allows you to switch on/off, adjust the brightness level, configure bottom push buttons and control various settings.

On the Control tab, select the dimmer, and then tap .

TIP: When you open the Device Control Screen for the first time, you will see an onboarding tip to help you configure the bottom push buttons of the dimmer.

The Device Control Screen displays the following options:

A

Drag the slider bar up/down to increase/decrease the brightness of your dimmer. For more information, refer to Adjusting the brightness.

B

Tap to turn the device on/off.

C

Tap to open the Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule.

D

Tap to configure the bottom push buttons by assigning an action or moment. For more information, refer to Configuring the bottom push buttons.

E

Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide.

F

Tap to open the Device Settings screen and configure the settings. For more information, refer to Configuring the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.