DUG_SysM - Connected Thermostat 2 A, ZB_WH-07

Removing the device

Using the Wiser Home app, you can remove the thermostat from the Wiser system.
To remove the thermostat from the Wiser system:
  1. On the Home page, tap .
  2. Tap Devices > > Delete (A).
  3. Read the confirmation message and tap Ok to remove the thermostat from the Wiser system.
    NOTE: By removing the thermostat, you will reset the thermostat. If you still have a problem with the reset, then refer to resetting the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?