DUG_SysM - Connected Thermostat 2 A, ZB_WH-07

Editing Schedule/Event

To edit the schedule:

  1. On the Home screen, tap .

  2. Tap Schedules tab and select the Schedule that you want to modify.

  3. Tap SCHEDULE DETAILS to do any of the following:

    • To rename the device

    • To change the device location

    • To delete Schedule

  4. To edit the EVENTS, select a day, and tap to change the time and temperature.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?