DUG_PowerTag-E_WH-09

Live

Using Wiser Home app, you can view the live data of power flow in your house (Grid import and export).
To view live data:
IMPORTANT: It is necessary to install PowerTag on Grid and additional power sources such as Solar, Solar and Battery to have accurate data of powerflow.
  1. On the bottom navigation bar, tap .
  2. Tap Live.
    • Grid import: The grid consumption with loads is represented in blue.
    • Grid import and export (Applicable for Grid with On Grid solar system): The grid consumption with loads is represented in blue and the excess energy of solar production sold is represented in green.

      The grid consumption with loads is represented in blue

      The excess energy of solar production sold is represented in green

    • Grid, Solar and Battery
      • Grid: Represented in blue.

      • Solar and Battery: Represented in green.

      Scroll down to view the graph.

      • Consumption total: It shows the total energy consumption in kWh.

      • Solar production: It shows the energy produced by the solar system in kWh.

      • Self-sufficiency: It shows the percentage of energy produced by the solar system that is consumed by the household.

      • % of production used: It shows the percentage of solar energy that is used.

    • Battery
      • Battery: Represented in black.

      • The battery's power value (charge and discharge in kW) and the percentage of the battery is shown one after the other.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?