DUG_Push-button Module, 1-gang/2-gang_WH-06

Opening/Closing the shutter using app

To open/close the shutter:
  1. On the Control tab, tap All devices or the room tab where the device is located.
  2. Tap (A) or (B) of the shutter or shutter slat to open/close it.
    TIP: You can also open/close the shutter or shutter slat:
    • By selecting of the shutter or shutter slat and using the slider in the device control screen to open/close it.

    • When you add it to your Favourites. To know more about Favourite, refer to Managing Favourite topic in the respective System User Guide.

      NOTE: If you only have a single device in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?