DUG_Smoke alarm DC_WH-01

Removing the device

Using the Wiser Home app, you can remove the device from the Wiser system.
To remove the device:
  1. On the Home page, tap .
  2. Tap Devices > Smoke Alarm > Delete (A).
  3. Tap OK to confirm.
    NOTE:
    • By removing the device, you will reset the device. The device blinks amber upon resetting, indicating that it is now ready to pair.

    • If you still have a problem with the reset, refer to Resetting the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?