DUG_Multiwire Puck Dimmer_WH–01

Setting Dimming Mode

Using the Wiser Home app, you can manage the Dimmer modes and settings.
  1. On the Home page, tap .
  2. Tap Devices > Micromodule Dimmer > Dimming Mode (A) and select either of the following options and tap Done.
    • RC Mode: When different load types are connected to the dimmer.
    • RL - LED Mode: When an LED is connected to the dimmer. Choose this mode only if the LED is not working properly in RC mode. Example, if you have problems with light flickering, changing the dimming mode to RL-LED improves the dimming quality.
      NOTE: RL - LED Mode uses 10 % of the nominal load to avoid overheating of the Dimmer, refer to Technical data.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?