SUG_Wiser_Home_Iberic_WH-08

Compatible Wiser Devices for Matter Bridge

Following are the Matter bridge compatible devices:

Refer to List of Wiser Devices for the links to Device user guide for each devices.

Sensors

Wiser Window/Door Sensor

Wiser Water Leakage Sensor

Wiser Motion Sensor

Wiser Temperature/Humidity Sensor

Lights

Wiser Micro Module Light Switch

Connected Relay Switch 10 A

Dimmers

Wiser Micro Module Dimmer
Wiser Multiwire Micro Module LED Dimmer
Connected Universal Rotary Dimmer LED
Connected Universal Push-button Dimmer LED

Shutters

Wiser Micro Module Shades Control

Connected Blind Control Switch

Appliances

Connected Single Socket Outlet

Wiser Plug

Connected Wireless Switch 1-gang/2-gang

Climate

Wiser Radiator Thermostat

Wiser Room Thermostat

Wiser Underfloor Heating Connection Strip

Safety

Wiser Smoke Alarm - Battery

Wiser Smoke Alarm 230 V

Energy

PowerTag E

PowerTag C

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.