SUG_Wiser_Home_Iberic_WH-09

Wiser HubR 2nd Generation

CCTFR6311G2

You can connect a heating or hot water system directly to the Wiser HubR 2nd Generation.

The app will guide you through the process to configure and add the devices to the system.

Once configured and added, the system connected to the Wiser HubR 2nd Generation will show up as a device in the app and can be configured and operated accordingly.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.