SUG_Wiser_Home_Iberic_WH-08

Appliances

Wiser Smart Plug

CCTFR6501

Remotely control and monitor the power consumption of the plugged-in load.

Instruction Sheet (PDF)

Device User Guide

Wiser Power Micromodule

CCTFR6730

The Wiser Power Micromodule hereinafter referred as module is for switching loads (up to 3000 W resistive) such as a hot water tank or a socket outlet.

In combination with the Wiser app, the energy consumption can be measured and the module can be used for load shedding or demand response.

Instruction Sheet (PDF)

Device User Guide

Connected Single Socket Outlet 16 A

NU5557xxW

NU5557xx

Control and monitor the power consumption of the plugged-in load.

Instruction Sheet (PDF)

Device User Guide)

Connected Wireless Switch 1-gang/2-gang

NU5571xxW

Battery powered push-button switch.

Buttons can be freely assigned with functions with the Wiser Home App.

Instruction Sheet (PDF)

Device User Guide

Connected single socket outlet 16A


MEG2380-0xxx
MEG2380-60xx

MTN2380-0xxx
MTN2380-60xx

Remotely control and monitor the power consumption of the plugged-in load.

Instruction Sheet (PDF)

Device User Guide

Connected Wireless Switch 1-gang/2-gang
MEG5001-0300

MTN5001-0300


MEG5001-6000

MTN5001-6000

Battery powered push-button switch.

Buttons can be freely assigned with functions with the Wiser Home App.

Instruction Sheet (PDF)

Device User Guide

Connected Push-Button module, 1-gang/2-gang


MEG5116-0300
MEG5126-0300

MTN5116-0300
MTN5116-6000


MEG5116-6000
MEG5126-6000

MTN5126-0300
MTN5126-6000

Control different inserts thru the push-buttons or the Wiser Home app.

To be combined with a blind control insert.

Instruction Sheet (PDF)

Device User Guide

Wiser SmartPlug 16 A

CCT711119

Controls various electrical devices, for example floor lamps, radios, ventilators or coffee machines, using the app. Monitor energy consumption of plugged-in devices.

Instruction Sheet (PDF)

Device User Guide

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?