Connecting to Wi-Fi®
Once you are connected to the hub's temporary Wi-Fi®network, enter the login information of your home Wi-Fi® into the hub.
To enter the Wi-Fi® login information:
-
Use the Wiser Home App as a Professional Installer or a Home owner.
-
Follow the steps in chapter Connecting to the Temporary Wi-Fi® Network of Hub
/Controller. -
When asked to connect your hub to your home Wi-Fi® network, tap Continue (A).
-
Select your Wi-Fi® network from the list.
NOTE: If your home network does not appear in the list of available network, tap Can‘t see your network? to allow you to manually enter your network credentials to easily connect to your home network. -
Enter the Wi-Fi® password and tap Join (B).
When the hub is connected to your Wi-Fi® network, you can start adding devices to your hub.
NOTE:-
The hub only operates in the 2.4 GHz range.
-
For more information about adding devices to the hub, refer to chapter Adding a Device.
-
Choose one of the following options:
-
Back to Homepage: Tap to return to the Home screen.
TIP: Tapto start adding devices to control your home. Refer to Adding a Device.
-
Add a New Device: Tap to start adding devices to control your home. Refer to Adding a Device.
-