SUG_Wiser_Home_Iberic_WH-08

Hubs

The Hub monitors and controls the Devices of your Home via the Wiser Home app, using Wi-Fi®.

Wiser Hub 2nd Generation

CCT501801

The Wiser Hub 2nd Generation monitors and controls the Devices of your Home via the Wiser Home App. It is connected to the Wiser Cloud for remote control via Wi-Fi®.

Instruction Sheet (PDF)

Getting to know the Hub

Wiser HubR 2nd Generation

CCTFR6311G2

The Wiser HubR is used to connect all the Wiser devices. This version is used where central heating (e.g. boiler or heat pump) is used.

Instruction Sheet (PDF)

Getting to know the Hub

Wiser Wall Box Power Supply

CCT501800-0001

Alternative power supply for the Wiser Hub 2nd Generation, placed in a wall box.

Instruction Sheet (PDF)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.