SUG_Wiser_Home_Iberic_WH-09

Changing home Wi-Fi login information

If you have made changes to your home Wi-Fi®, you need to apply those changes to the hub.

The Wiser app will detect that the connection to the hub is lost and suggest solutions.

To change the Wi-Fi® information in the hub:

  1. Tap I’ve changed my Wi-Fi router (A).

The app will guide you through the process of selecting a Wi-Fi® network and entering the password.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.