SUG_Wiser_Home_Iberic_WH-08

Climate

Wiser Radiator Thermostat

CCTFR6100

Provides individual temperature control for radiators.

Instruction Sheet (PDF)

Device User Guide

Wiser Room Thermostat with display

CCTFR6400

Wireless, battery-powered, colored touch-button display to set the room temperature.

Instruction Sheet (PDF)

Device User Guide

Wiser Flush-mounted Thermostat 2 A


CFMT02ZB

The Wiser Flush-mounted Thermostat 2 A is mainly used for water-based heating and cooling applications, such as water-based underfloor heating and radiator heating.

NOTE:The thermostat is not suitable for directly connecting an electrical heating.

Instruction Sheet (PDF)

Device User Guide

Wiser Underfloor Heating Connection Strip

CCTFR6600

Control thermal actuator valve heads to regulate the flow of hot water in the underfloor pipes.

Instruction Sheet (PDF)

Device User Guide

Wiser Boiler Relay

CCTFR6001

Allows control of a domestic boiler in water based central heating applications.

IMPORTANT: The Wiser Boiler Relay is not compatible with the Wiser HubR 2nd Generation.

Instruction Sheet (PDF)

Device User Guide

Wiser 16 A Relay for Temperature Control

CCTFR6700

Control electrical heaters with On/Off commands (Relay output) or Fil Pilote commands.

Instruction Sheet (PDF)

Device User Guide

Third party devices

Devices that are compatible with a Wiser System, but are not provided by Schneider Electric.

Airzone Plenum

Zoning system for HVAC (heating, ventilation, and air conditioning) used in buildings that regulates the indoor temperature.

Device User Guide

Aidoo Pro Air conditioner

It is a solution that lets you control individual air conditioner through the Wiser Home app. An Aidoo Pro Air conditioner is wired to the AC and connects to the Wiser Home app via Wi-Fi®.

Device User Guide

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?