SUG_Wiser_Home_Iberic_WH-09

Operating Elements

A Setup

Activates the temporary Wi-Fi® network of the Hub. It is used during the commissioning process and troubleshooting.

B Heating Override*

Turning on the heating override will turn on the connected heating system for 2 hours regardless of any settings in the app or thermostats.

To start override: press and hold button for more than 3 seconds.

To stop override, short press the button.

* NOTE: The heating override switches off when the temperature is close to set point. However, in the app, the heating flame symbol will continue to display until the set point is reached. This is normal operation and will not affect the heating.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.