DUG_Radiator Thermostat_WH-07

Operating the device using the Wiser Home app

In the Wiser Home app, the device control screen allows to switch ON/OFF the device and control it.

On the Control tab, select the thermostat.

The device control screen displays the following options:

A

Tap the toggle switch allow the system to follow a schedule.

B

Tap to redirect you to the Schedule screen, where you can create a schedule.

C

Tap to add the device to the Favorite devices section in the Home screen. When you add it to your Favourites. To know more about Favourites, refer to the Managing Favourites topic in the respective System User Guide.

D

Tap to control various settings from the Device Settings screen.

E

Tap to manually turn the device ON/OFF.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?