DUG_Radiator Thermostat_WH-07

Pairing the device with the Wiser hub

Using the Wiser Home app, pair your Thermostat with the Wiser Hub to access and control.
To pair the Thermostat:
  1. On the Home screen, tap .
  2. Tap Devices > and tap Climate > Radiator Thermostat.
    TIP:
    • You can also navigate by tapping Control > > Climate > Radiator Thermostat.

    • The next screen shows the joining process of the Thermostat.

  3. Twist and hold the Thermostat cap in the “+” direction.
    After 3 seconds, LED flashes green.
    In the app, you can see the Thermostat is successfully joined.

  4. Tap Next to enter Thermostat name and assign to an existing room or a new room.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

The Thermostat is now listed on the Control tab under the All and the specific room tabs.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?