DUG_Radiator Thermostat_WH-07

Identifying the device

Using the Wiser Home app, you can identify a Thermostat from the other available devices in the room.
To identify the Thermostat:
  1. On the Home screen, tap .
  2. Tap Devices > Radiator Thermostat > Identify (A).
    NOTE:
    • This feature flashes the Thermostat LEDs, so you can identify the actual device. It may take up to a minute to start and flash the Thermostat LED.

    • The Thermostat LEDs will continue to flash until you tap OK.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?