0102CT2001

Connected Products

Wi-Fi Connected Wiring Devices

Give customers the elegant, minimalist look they want, with the connectivity they need to save energy and live comfortably. These wiring devices retain the classic functionality of traditional light switches, outlets, and wall plates, while featuring modern aesthetic and intelligent IoT connectivity. Ideal for hub-free new construction and residential upgrades.

Schneider Home

Schneider Home by Schneider Electric App

Experience Schneider Home, the gateway to your Schneider Electric Smart Home.

Schneider Home allows for the addition, configuration, control, and scheduling connected Schneider Electric devices from anywhere. Use the built-in energy monitoring feature to identify devices that tend to overuse energy in your home, and take action to reduce your utility bill.

  • Single app for commissioning, remote control and operation of Wi-Fi devices on the network.

  • Simplifies the Wi-Fi setup process without sacrificing security by using QR codes.

  • Integrates with a complete portfolio of Wi-Fi enabled Dimmers, Switches, Receptacles and Plug-In Receptacles that have built-in energy monitoring.

  • Controls lights from anywhere, no hub required.

  • Ability to create rooms and add devices from easy visibility across the entire house.

  • Shows real time energy usage, and ability to schedule devices from a single screen. Offers scheduling routines at specific times or based on sunrise/sunset.

  • Offline mode allows for App control while at home if the internet is down.

  • Identifies devices that tend to overuse energy in the home and take action to reduce your utility bill.

  • Features such as Moments allow us to control and schedule a group of devices.

  • Supports popular voice assistants from Amazon and Google for more comprehensive automation.

  • Allows in-built integration with Schneider Energy Monitor that provides homeowners with easy-to-understand, app-based information about how their home uses electricity so they can make informed decisions to reduce their energy consumption.

  • Schneider Energy can monitor multiple loads on a single circuit – monitoring energy consumption down to the device level.

Schneider Home App

Amazon, Alexa and all related logos are trademarks of Amazon.com, Inc. or its affiliates.
Google and Google Nest Audio are trademarks of Google LLC.

SQR226U1LAW

X Series 600 Watt Single-Pole / 3-Way Wi-Fi Energy Monitoring Rocker Dimmer Back Wire Clamps

  • Dimmer based on 2.4 GHz Wi-Fi platform which connects directly to the home network. No hub required.

  • Part of Schneider Electric’s grid-to-plug initiative combining control and monitoring of the entire home electrical infrastructure.

  • Supports single-pole and 3-way (multi-way) wiring scenarios for flexible installation.

  • Cost effective 3-way expansion using a single-pole switch on the far end connected to the traveler and neutral wires.

  • Simplified but secure QR Code based installation process.

  • Energy monitoring built-in to track consumption at point of use.

  • Wi-Fi Certified ensures set-up with certified routers and mesh networks as well as support for the latest security protocols.

  • Schedules are stored in the device and will execute even if the internet is down.

  • Works with Schneider Energy Monitor by Schneider Electric.

  • Back wire pressure plates allows for up to two #12 copper solid or stranded wires to be securely captured for flexible installation.

  • Grounding screw pressure plate speeds ground wire installation.

  • Combo screw heads accept slotted, Phillips®, and Robertson Square® tools.

  • Neutral wire is required for operation.

  • RoHS compliant.

  • High impact-resistant, matte, non-glossy, easy-to-clean thermoplastic body for attractive long-lasting operation.

  • Available in White (WH), Light Almond (LA), and Black (BK).

  • 2-year product warranty.

SQR141U1BKW

X Series 15 A Single-Pole / 3-Way Wi-Fi Energy Monitoring Rocker Switch Back Wire Clamps

  • Switch based on 2.4 GHz Wi-Fi platform which connects directly to the home network. No hub required.

  • Part of Schneider Electric’s grid-to-plug initiative combining control and monitoring of the entire home electrical infrastructure.

  • Supports single-pole and 3-way (multi-way) wiring scenarios for flexible installation.

  • Cost effective 3-way expansion using a single-pole switch on the far end connected to the traveler and neutral wires.

  • Simplified but secure QR Code based installation process.

  • Energy monitoring built-in to track total consumption of devices plugged into switched outlets.

  • Wi-Fi Certified ensures set-up with all certified routers and mesh networks as well as support for the latest security protocols.

  • Schedules are stored in the device and will execute even if the internet is down.

  • Works with Schneider Energy Monitor by Schneider Electric.

  • Back wire pressure plates allows for up to two #12 copper solid or stranded wires to be securely captured for flexible installation.

  • Grounding screw pressure plate speeds ground wire installation.

  • Combo screw heads accept slotted, Phillips, and Robertson Square tools.

  • Neutral wire is required for operation.

  • RoHS compliant.

  • High impact-resistant, matte, non-glossy, easy-to-clean thermoplastic body for attractive long-lasting operation.

  • Available in White (WH), Light Almond (LA), and Black (BK).

  • 2-year product warranty.

SQR441U1WHW

X Series 15 A 125 Volt Tamper Resistant Wi-Fi Energy Monitoring Duplex Receptacle Back Wire Clamps

  • Receptacle based on 2.4 GHz Wi-Fi platform which connects directly to the home network. No hub required.

  • Part of Schneider Electric’s grid to plug initiative combining control and monitoring of your entire home electrical infrastructure.

  • Simplified but secure QR Code based installation process.

  • Only one outlet is controllable, however, energy monitoring is built-in to both outlets to track total receptacle consumption.

  • Wi-Fi Certified ensures set-up with all certified routers and mesh networks as well as support for the latest security protocols.

  • Schedules are stored in the device and will execute even if the internet is down.

  • Works with Schneider Energy Monitor by Schneider Electric.

  • Back wire pressure plates allows for up to two #12 copper solid or stranded wires to be securely captured for faster flexible installation.

  • Grounding screw pressure plate speeds ground wire installation.

  • Combo screw heads accept slotted, Phillips, and Robertson Square tools.

  • Neutral wire is required for operation.

  • RoHS compliant.

  • High impact-resistant, matte, non-glossy, easy-to-clean thermoplastic body for attractive long-lasting operation.

  • Available in White (WH), Light Almond (LA), and Black (BK).

  • 2-year product warranty.

SQR621U1WHW

X Series 15 A 125 Volt Wi-Fi Energy Monitoring Plug-In Receptacle

  • Receptacle based on 2.4 GHz Wi-Fi platform which connects directly to the home network. No hub required.

  • Part of Schneider Electric’s grid-to-plug initiative combining control and monitoring of your entire home electrical infrastructure.

  • Simplified but secure QR Code based installation process.

  • Energy monitoring is built-in to track consumption.

  • Wi-Fi Certified ensures hassle free set-up with all certified routers and mesh networks as well as support for the latest security protocols.

  • Schedules are stored in the device and will execute even if the internet is down.

  • Works with Schneider Energy Monitor by Schneider Electric.

  • RoHS compliant.

  • High impact-resistant, matte, non-glossy, easy-to-clean thermoplastic body for attractive long-lasting operation.

  • 2-year product warranty.

Z-Wave Plus Wiring Devices

This line of connected wiring devices is certified by the Z-Wave Alliance and is designed to support home automation and security systems chosen by home builder’s or their technology partner’s residential projects. These products require a Z-Wave Alliance certified hub to work.

SQR22102WHZ

X Series 600 Watt Single-Pole / 3-Way Z-Wave Plus Energy Monitoring Rocker Dimmer Back Wire Clamps

For use in areas where variable lighting is a requirement–such as a living room–where you want bright light for reading on the couch, but dim lighting for watching a movie. Ideal for monitoring energy usage and determining cost savings associated with dimming lights.

  • Dimmer supports S2 SmartStart allowing the connection to the hub prior to installing at the jobsite.

  • Energy monitoring built-in to track consumption at point of use.

  • Dims both Incandescent and LED loads.

  • Supports single-pole and 3-way (multi-way) wiring scenarios for flexible installation.

  • 3-way expansion requires the use of the Z-Wave Remote Switch/Dimmer.

  • Dimmer can be grouped with up to five other Z-Wave Plus devices.

  • Back wire pressure plates allows for up to two #12 copper solid or stranded wires to be securely captured for faster flexible installation.

  • Z-Wave certified to work with most hubs.

  • Grounding screw pressure plate speeds ground wire installation.

  • Combo screw heads accept slotted, Phillips, and Robertson Square tools.

  • Neutral wire is required for operation.

  • RoHS compliant.

  • High impact-resistant, matte, non-glossy, easy-to-clean thermoplastic body for attractive long-lasting operation.

  • Available in White (WH), Light Almond (LA), and Black (BK).

  • 2-year product warranty.

SQR14102BKZ

X Series 15 A Single-Pole / 3-Way Z-Wave Plus Energy Monitoring Rocker Switch Back Wire Clamps

The switch is the professional’s choice for reliable lighting control. Sensitive enough to control the low wattage demands of a single LED yet also capable of the demands placed by bright outdoor lighting. Ideal for monitoring energy usage in bedrooms where the switch controls the receptacles.

  • Switch supports S2 SmartStart allowing the connection to the hub prior to installing at the jobsite.

  • Supports single pole and 3-way (multi-way) wiring scenarios for flexible installation.

  • 3-way expansion requires the use of the Z-Wave Remote Switch/Dimmer.

  • Switch can be grouped with up to five other Z-Wave Plus devices.

  • Grounding screw pressure plate speeds ground wire installation.

  • Back wire pressure plates allows for up to two #12 copper solid or stranded wires to be securely captured for faster flexible installation.

  • Combo screw heads accept slotted, Phillips, and Robertson Square tools.

  • Neutral wire is required for operation.

  • RoHS compliant.

  • High impact-resistant, matte, non-glossy, easy to clean thermoplastic body for attractive long-lasting operation.

  • Available in White (WH), Light Almond (LA), and Black (BK).

  • 2-year product warranty.

SQR50101WHZ

X Series 15 A Z-Wave Remote Rocker Switch/Dimmer Back Wire Clamps

The remote switch/dimmer does not control a load and is used primarily as the secondary device in a 3-way lighting scenario. The remote can also pair with a receptacle or plug-in outlet to virtually create a switched outlet for floor lamps.

  • Remote supports S2 SmartStart™ allowing the connection to the hub prior to installing at the jobsite.

  • This device does not control a load.

  • Required for 3-way expansion of either the Z-Wave Switch or Dimmer.

  • Can also be used to pair with a Z-Wave Receptacle or Plug-In Outlet to create a switched outlet.

  • Remote can be grouped with up to five other Z-Wave Plus devices.

  • Grounding screw pressure plate speeds ground wire installation.

  • Back wire pressure plates allows for up to two #12 copper solid or stranded wires to be securely captured for faster flexible installation.

  • Combo screw heads accept slotted, Phillips, and Robertson Square tools.

  • Neutral wire is required for operation.

  • Complies with California Title 24.

  • RoHS compliant.

  • High impact-resistant, matte, non-glossy, easy-to-clean thermoplastic body for attractive long-lasting operation.

  • Available in White (WH), Light Almond (LA), and Black (BK).

  • 2-year product warranty.

SQR44102LAZ

X Series 15 A 125 Volt Tamper Resistant Z-Wave Plus Energy Monitoring Duplex Receptacle Back Wire Clamps

For use in areas where you want to control a device that is not connected to a switch. The receptacle mounts inside the electrical box like a standard outlet so it blends into the home. Ideal for monitoring energy usage of the device plugged into the controlled outlet.

  • Receptacle supports S2 SmartStart allowing the connection to the hub prior to installing at the jobsite.

  • One outlet is controllable; however, energy monitoring is built-in to both outlets to track total receptacle consumption.

  • Receptacle can be grouped with up to five other Z-Wave Plus devices.

  • Z-Wave certified to work with most hubs.

  • Back wire pressure plates allows for up to two #12 copper solid or stranded wires to be securely captured for faster flexible installation.

  • Grounding screw pressure plate speeds ground wire installation.

  • Combo screw heads accept slotted, Phillips, and Robertson Square tools.

  • Neutral wire is required for operation.

  • RoHS compliant.

  • High impact-resistant, matte, non-glossy, easy-to-clean thermoplastic body for attractive long-lasting operation.

  • Available in White (WH), Light Almond (LA), and Black (BK).

  • 2-year product warranty.

SQR226U1WHW SQR22102WHZ  

Connected products

Technology Electrical Rating Device Type Three Way Remote Nominal Load 1 Load Type 1 Nominal Load 2 Load Type 2 Color (Matte) Catalog Number
Wi-Fi Connected Dimmer – Residential
2.4 GHz Wi-Fi 5 A / 120 V Multi-way Single Pole Switch 600 W Halogen, Incandescent 150 W Dimmable LED White

SQR226U1WHW

Light Almond

SQR226U1LAW

Black

SQR226U1BKW

Z-Wave Connected Dimmer – Residential
Z-Wave Plus 5 A / 120 V Multi-way Remote Switch / Dimmer 600 W Halogen, Incandescent 150 W Dimmable LED White

SQR22102WHZ

Light Almond

SQR22102LAZ

Black

SQR22102BKZ

SQR141U1WHW SQR14102WHZ SQR50101WHZ
Technology Electrical Rating Device Type Three Way Remote Color (Matte) Catalog Number
Wi-Fi Connected Switch – Residential
2.4 GHz Wi-Fi 15 A / 120 V Multi-way Single Pole Switch White

SQR141U1WHW

Light Almond

SQR141U1LAW

Black

SQR141U1BKW

Z-Wave Connected Switch – Residential
Z-Wave Plus 15 A / 120 V Multi-way Remote Switch / Dimmer White

SQR14102WHZ

Light Almond

SQR14102LAZ

Black

SQR14102BKZ

Z-Wave Connected Remote Dimmer Switch – Residential
Z-Wave Plus 15 A / 120 V Multi-way Remote / No Load Control White

SQR50101WHZ

Light Almond

SQR50101LAZ

Black

SQR50101BKZ

SQR441U1WHW
SQR44102WHZ
Technology Electrical Rating Device Type Color (Matte) Catalog Number
Wi-Fi Connected Receptacle – Residential – Tamper Resistant
2.4 GHz Wi-Fi 15 A / 125 V Duplex White

SQR441U1LAW

Light Almond

SQR441U1WHW

Black

SQR441U1BKW

Z-Wave Connected Receptacle – Residential – Tamper Resistant
Z-Wave Plus 15 A / 125 V Duplex White

SQR44102WHZ

Light Almond

SQR44102LAZ

Black

SQR44102BKZ

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.