0102CT2001

Screwless Wall Plates

X Series 1-5 Gang Standard Size Screwless Wall Plate

  • Screwless, matte, non-glossy wall plate offers a clean, flush profile.

  • One-piece sub-plate screws align devices to ensure proper positioning of the wall plate.

  • Securely mounts to sub-plate and is easily removed by pressing a button on the bottom of the cover.

  • Standard size wall plate tightly frames the wiring device for sleeker appearance.

  • Made of rugged, washable thermoplastic for years of use.

  • Available in White (WH), Light Almond (LA), Black (BK), and Gray (GY).

  • RoHS Compliant, cULUs and UL514D compliant.

  • 2-year product warranty.


See Mid-Size Plus Wall Plates for dimensions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.