0102CT2001

Richer Features

  X Series Front
X Series Back
 
A Black tamper-resistant shutters – Put safety at the forefront without making it obvious, with easy-sliding shutters
B Side-mount pressure plates – Speed wiring time with better accessibility
C Self-grounding clip – Skip the separate grounding screw
   
   
   
   
   
A Grounding wire hole – Install faster utilizing this innovation for quickly wrapping the grounding wire to the grounding screw
B Bigger cutout for wire snips – Enjoy easy-access cutout space for speedy wire snips
C Wire push-in – Connect wire quickly with the push-in option and avoid the need to wrap

Receptacles offer multiple installation methods such as back wiring, backstabbed, and side wiring options to meet the installer’s preferences. These options ensure a seamless installation process regardless of the experience level of the installer.


Installation method
There are three types of installation methods.

All devices are cULus, RoHS Compliant

cULus: All devices are tested to meet the safety standards of Canada and United States by Underwriters Laboratories.

RoHS/Reach certified: Breathe easy with safe, non-hazardous materials.

Plastics: Extend product lifetime with super-durable polycarbonate resin.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.