0102CT2001

Fan Controls

SQR31103GY
SQR31103WH

X Series 2.5 A 3–Speed Slide Fan Controller Back Wires

  • Slide control provides clear user feedback as to which of the three positions are engaged.

  • Quiet 2.5 A fan motor control.

  • Rear wires with clear identification make for quick connection to electrical system.

  • RoHS compliant.

  • High impact-resistant, matte, non-glossy, easy to clean thermoplastic body for attractive long lasting operation.

  • Available in White (WH), Light Almond (LA), Black (BK), and Gray (GY).

  • 2-year product warranty.





Fan Controls

Electrical Rating Device Interface Speed Types Color (Matte) Catalog Number
Fan Speed Controller – Residential
2.5 A Slide 3 White

SQR31103WH

Light Almond

SQR31103LA

Black

SQR31103BK

Gray

SQR31103GY

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.