1600CT1901

NF Panelboard Features and Benefits

A broad range of NF panelboard kits are available ready to install (RTI) from stock to address common electrical distribution needs up to 600Y/347 Vac. Details of the NF RTI Panelboard offer may be found in Tables 9.46 - 9.48 and Tables 9.75 - 9.81 of Digest 178. Custom OEM solutions are also available to meet repetitive needs for unique panelboard configurations.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.