Add Buttons to the Toolbar

You can add any of the buttons listed in the ArcFM Solution Toolbar topic to your toolbar. To add buttons to your toolbar, perform the following steps:

  1. Right-click the gray area of the toolbar and select Customize.
  2. Select the Commands tab and click ArcFM Solution.
  3. Drag icons from Commands and drop them on the toolbar.
  4. Right-click the gray area of the toolbar and select Customize.
  5. Drag the button from the toolbar and drop it anywhere off the toolbar.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.