ArcFM Solution Licensing

The ArcFM Solution suite of tools offers a wide variety of licensing options to accommodate any type of user.

Product

License

Esri License

Description

ArcFM

ArcFM

ArcGIS for Desktop Standard

Tools for managing, modeling and editing facility and landbase data in an enterprise system.

Designer

Designer

ArcGIS for Desktop Standard

An integrated environment for preparing construction work sketches and job cost estimates.

Fiber Manager

ArcFM, Fiber Manager Extension

ArcGIS for Desktop Standard

An integrated set of tools used to display, manage, and analyze the fiber optic networks within a network system.

Responder Client

Responder Dispatcher

ArcGIS for Desktop Basic

Portion of Responder that provides access to Responder Explorer and Archive Explorer tools.

Responder Server

Responder Dispatcher

ArcGIS for Desktop Basic

Responder Services such as prediction, data services, and archive services.

Responder Web

None

ArcGIS for Server

Web-based call entry and reporting for the Responder outage management system.

ArcFM Viewer

ArcFM Viewer

ArcGIS for Desktop Basic

Built on ArcFM Desktop, this application provides query and display tools for ArcFM data.

ArcFM Viewer for ArcGIS Engine

ArcFM Viewer for ArcGIS Engine

ArcGIS Engine Runtime or ArcGIS for Desktop Basic

Built using ArcFM Engine development tools, this application allows the user to query and display ArcFM data.

Fiber Viewer for ArcGIS Engine

ArcFM Viewer for ArcGIS Engine

ArcGIS Engine Runtime or ArcGIS for Desktop Basic

An integrated set of tools used to to view fiber optic network data and produce reports.

ArcFM Inspector

ArcFM Viewer for ArcGIS Engine and Inspector extension

ArcGIS Engine Runtime

View, query, make redline edits, edit non-spatial attributes to feature classes.

ArcGIS Engine Runtime, Geodatabase Update Extension

View, query, make redline edits, edit attributes on various classes (including relationship classes, feature-linked annotation, dimension feature classes and custom feature classes).

Conduit Manager

ArcFM, Conduit Manager extension

ArcGIS for Desktop Standard

Manage underground facilities such as conduit and manholes.

Redliner

ArcFM Viewer for ArcGIS Engine, Redliner extension

ArcGIS Engine Runtime or ArcGIS for Desktop Basic

Graphic markup (redlining) within ArcFM Viewer for ArcGIS Engine and the ArcFM Mobile Solution.

ArcFM Viewer, Redliner extension

ArcGIS for Desktop Basic

Graphic markup (redlining) within ArcFM Viewer and the ArcFM Mobile Solution

Network Adapter

ArcFM, Network Adapter extension

ArcGIS for Desktop Standard

Integrate engineering analysis tools with the ArcFM Solution.

ArcFM Engine

ArcFM Engine

ArcGIS Engine

Develop a custom application for viewing ArcFM data in an enterprise system.

ArcFM Engine Developer Kit

ArcFM Engine, ArcFM Viewer for ArcGIS Engine

ArcGIS Engine SDK, ArcGIS Engine Runtime

Provides the tools necessary to build custom ArcFM Engine applications.

ArcFM Engine Runtime

ArcFM Engine

ArcGIS Engine Runtime

Necessary to run custom ArcFM Engine tools.

ArcFM Server

ArcFM Server

ArcGIS for Server

Core geodatabase management tools and technology for data storage, management, and distribution (Web-based data replication).

ArcFM for Silverlight

None

None

Provides a web application that allows you to view and navigate GIS data.

ArcFM for Silverlight SDK

None

None

Provides the tools necessary to create a custom web application that uses ArcFM Server.

ArcFM Object Reader

None

None

Provides the capability to view ArcFM objects.

Designer Express

Designer Express

ArcGIS for Desktop Standard

A less complex version of Designer which provides tools for preparing construction work sketches and job cost estimates.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.