Change Attribute Field Order

Use the Field Display tab of the ArcFM Properties Manager to change the order of attribute fields as they appear on the Attribute Editor.

  1. Select a feature class in ArcCatalog.
  2. Click the Properties Manager button on the ArcFM Solution toolbar, or right-click the feature and select ArcFM Properties Manager from the context menu.
  3. Click the Field Display tab, and then select a field to move.
  4. Move the field up or down using the arrow buttons at the right of the screen to reorder the field.
  5. Click Apply to save edits on any of the tabs and retain the Properties Manager.
  6. Continue to reorder fields or edit properties as needed.
  7. Click OK to save changes and dismiss the Properties Manager.

    Attributes are listed on the Attribute Editor in the order you defined.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.