Run the ArcFM Solution Object Converter

  1. Select the objects, feature classes, feature datasets, or geodatabases that you want to convert.
  2. On the ArcFM Solution toolbar, select the ArcFM Solution Object Converter button.
    You can press the Esc key to dismiss the Object Converter dialog.
  3. Select the format to which you want to convert the object(s) or geodatabase.

  4. Click OK.
  5. Do one of the following depending on the message you receive:
    • If you receive a message indicating that the object has already been converted to your selected format, click OK.

    • If you receive a message indicating that the object has not already been converted, click Yes if you want to continue the conversion.

      A status bar indicates the progress of the conversion. To cancel the object conversion before it has completed, press the Esc key.

  6. When a confirmation message appears indicating that the object has been successfully converted, click OK.
    IMPORTANT: Changing the GUIDs of objects is significant. Objects converted with this tool are only viewable with ArcFM Solution products. A free program called ArcFM Solution Object Reader is available for viewing converted objects on machines where ArcFM Solution products are not installed. For more information, please visit Schneider Electric Support.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.