Create the Exclusive SDE Connection

The standalone executable requires an exclusive SDE connection to the geodatabase. This connection should only be used for the executable and not for any other administrative purposes.
  1. Open ArcCatalog.
  2. In the Catalog Tree > Database Connections, double-click Add Database Connection.

  3. In the Database Connection dialog, populate all fields to create an SDE connection to your geodatabase.
  4. Check the box to save user name and password. This is required by the executable.

  5. Click OK.
  6. As a recommendation, rename your connection to clearly indicate it is the connection to be used exclusively by the executable.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.