Workflow Manager Data Source Wizard

The Workflow Manager Data Source Wizard allows you to change the data sources for design workspaces (Designer only). You may want to first use the ArcFM Data Source Wizard to convert the data sources for design stored displays first.

IMPORTANT: Once you have begun updating data sources, the tool cannot be stopped, cancelled, or undone. Schneider Electric strongly recommends that you back up the MM_WMS_DESIGNS table prior to using the Workflow Manager Data Source Wizard.

The Workflow Manager Data Source Wizard is installed in the ArcFM Solution\bin directory. Look for: WorkflowManagerDataSourceWizard.exe. Double-click the .exe file to open it.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.