Grid Dimension Fields

For each fiber point facility, map the Wavepoint XI fields to the equivalent fields in your database. The names in the animated demonstration are examples, and your names differ depending on your database.


When mapping fields, keep the following in mind:

  • The application only reveals relevant fields per point facility, and it grays out fields that do not pertain to the chosen point.

    • If all fields are gray, you do not need to map anything. This is the case with BackPort, ActiveSplitPort, DevicePoint, PatchLocation, Shelf, Splice, and Splitter. These either do not need to be rendered, or they borrow their position from a sibling relationship (BackPort, for example, follows the field mapping for FrontPort).

  • To revert a field back to “Unassigned,” click the X next to the menu.

  • After mapping fields, always click Save.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?