The Published Map Service

Wavepoint XI uses the same published fiber map service as Fiber Manager XI. Thus, pay particular attention to Publishing the Fiber Map Service, as it is used by both applications.

When you Add Operational Map to Solution Center, enable the Wavepoint toggle.

If you are a Wavepoint Classic customer, it is helpful to have your Wavepoint web.config file handy. You do not necessarily have to replicate all your previous configurations, but the file helps you understand the choices in Solution Center that mirror the previous configurations in Wavepoint Classic.


Also make sure to check the Fiber Manager Relationships in ArcGIS Pro.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?