Line Field Mappings

For each fiber line asset, map the Wavepoint XI fields to the equivalent fields in your database.

When mapping fields, keep the following in mind:

  • To revert a field back to “Unassigned,” click the red icon.

  • After mapping fields, always click Save.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?