Port Fields

For each fiber port facility, map the Wavepoint XI fields to the equivalent fields in your database.

When mapping fields, keep the following in mind:

  • The application only reveals relevant fields per point facility, and it grays out fields that do not pertain to the chosen point.

    • If all fields are gray, you do not need to map anything. This is the case with sibling relationship (BackPort, for example, follows the field mapping for FrontPort).

  • To revert a field back to “Unassigned,” click the red icon.

  • After mapping fields, always click Save.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?