DOCA0140EN-03

Protection Against Ground Faults

Introduction

Protection against ground faults is provided by:

  • Earth-leakage protection in the case of low intensity fault currents (fault current limitation is linked to ground connection diagram TT or TN-S). Earth-leakage protection is provided by:

    • Earth-leakage protection embedded in MicroLogic 4 and 7 trip units.

    • VigiPacT Add-on earth-leakage protection module added to the circuit breaker.

  • Ground-fault protection embedded in MicroLogic 6 trip units in the case of high intensity fault currents (this protection can be used only with ground connection diagram TN-S)

Embedded Earth-Leakage Protection

Earth-leakage protection is embedded within the MicroLogic 4 and 7 trip units.

The maximum value of IΔn depends on the circuit breaker frame size:

Circuit breaker frame size

100 - 250

400 - 630

Maximum value IΔn

5 A

10 A

The range provides two types of device:

  • Trip devices trip on an earth-leakage fault

  • Alarm devices measure and signal an earth-leakage fault without tripping:

    • On the front face

    • Through the SDx output contact

The following illustrations show the two types of MicroLogic 4 trip units:

MicroLogic 4 trip

MicroLogic 4 alarm

For more information about MicroLogic 7, refer to DOCA0141EN, ComPact NSXMicroLogic 5/6/7 Electronic Trip Units - User Guide.

Earth-Leakage Protection with VigiPacT Add-on

The VigiPacT Add-on is external to the trip unit and is designed to provide earth-leakage protection for the following situations:

  • For system voltages up to 550 Vac

  • For breaking capacity over 150 kA

The VigiPacT Add-on can be installed on ComPact NSX circuit breakers with thermal, thermal-magnetic, or MicroLogic 2, 5, and 6 trip units.

Illustration of VigiPacT Add-on installed on a ComPact NSX circuit breaker

Ground-Fault Protection

Ground-fault protection is embedded in MicroLogic 6 trip units. For more information, refer to DOCA0141EN, ComPact NSXMicroLogic 5/6/7 Electronic Trip Units - User Guide.

Setting the Earth-Leakage Protection

Installation standards require or recommend particular sensitivity and trip time values for earth-leakage protection:

Type of protection

IΔn

Δt

Installation standards

Protection against direct contact

≤ 30 mA

≤ 40 ms (1)

Required

Fire protection

≤ 300 mA or ≤ 500 mA

≤ 40 ms (1)

Required if necessary

Protection against indirect contact

IΔn

≤ 1 s

Lowest possible recommended values of IΔn and Δt (the value of IΔn depends on the ground resistance)

(1) Value of Δt for a fault current ≥ 10 IΔn

Setting the Ground-Fault Protection

Installation standards (in particular the NEC - National Electrical Code - defining installation rules in the USA) require or recommend the pickup and trip time values for ground-fault protection.

Location

Ig

tg

NEC

On the incoming supply to the low voltage distribution (and for In > 1,000 A)

≤ 1,200 A

Required

≤ 3,000 A

≤ 1 s

Required

Downstream of the low voltage distribution

Ig

Lowest possible recommended values for Ig

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?