0100DB1615

Changes to Section 19: Push Buttons and Operator Interface

Printed Book Page Number(s)

Current PDF Page Number(s)

Topic(s)

Reason for Change

Specific Change Made

Change Date

19-31

19-31

XB4 Specialty Operators

New table

Added fully-assembled 22 mm XB4 metal potentiometers. Table titled “Complete Potentiometers” This is table 19.84 in June 2017 PDF.

Jun-2017

19-31 through 19-51

19-31 through 19-51

Table title numbers changed.

A new table was added to page 19-31. This has adjusted (by 1) the numbering of all tables in the printed book starting with table 19.84.

Jun-2017

19-45

19-45

XB5 Complete Devices

New

Added multiple new monolithic pilot lights in existing XB5 range - Table titled “Pilot Lights with Protected LED (screw clamp terminal connections)” Table 19.132 in June 2017 PDF

Jun-2017

19-51

19-51

XB5 Specialty Operators

New table

Added XB5 metal potentiometers. Table titled “Complete Potentiometers”. This is table 19.148 in June 2017 PDF.

Jun-2017

19-51 through 19-114

19-51 through 19-114

Table title numbers changed.

A new table was added to page 19-51. This has adjusted (by 2) the numbering of all tables in the printed book starting with table 19.148.

Jun-2017

19-72

19-72

Type K Heavy Duty Operators

Correction

Table 19.214 titled "Non-Illuminated Momentary Push Button Operators": table sub headings added to for the rows containing 9001KR4B and 9001KR5B images.

Mar-2016

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.