990-66233C-001

Overview of Single UPS

UIB Unit input disconnect device
SSIB Static switch input disconnect device
UOB Unit output disconnect device
MBB Maintenance bypass disconnect device
BB1 Battery disconnect device 1
BB2 Battery disconnect device 2
NOTE: In Schneider Electric literature, 'disconnect device' is used as a generic term covering circuit breakers or switches as their position may vary depending on configuration. Details about the individual configuration are found in the electrical diagram and/or by reading the symbol on the front of each disconnect device.
NOTE: Ensure that any external battery matches the internal battery’s type and configuration. Schneider Electric offers modular battery modules such as E3SXR6, which are factory-tested to work with the provided internal batteries. To order E3SXR6 or verify compatibility, please contact Schneider Electric.