990-66233D-001

Communication and Management

Modbus Modbus (RTU)
Output relays 3 x SELV configurable
Input contacts 3 x SELV configurable
Standard control panel 5 inch touchscreen display
Audible alarm Yes
Emergency power off (EPO)

Options:

  • Normally Closed (NC)

Internal switch

UIB
UOB
SSIB
MBB
BB (Only applicable for UPS for internal batteries)

Battery monitoring Available for external battery solutions