990-66233C-001

Leakage Current

UPS rating Leakage current at 100% load (mA)
10 kVA

250

15 kVA

250

20 kVA

250

30 kVA

100

40 kVA

100

NOTE: As per IEC 62477-1, the leakage current should not exceed 5% of the rated input current.