990-66230A-001

Alarm Messages

Display text Description Corrective action
Air filter check required The air filter service life has expired and requires a check. Replace the air filter.
Battery boost charging The batteries are charged with the configured boost charge voltage.  
Battery connected The batteries are connected.  
Battery discharging The load is drawing more power than the UPS can draw from the input, causing the UPS to draw power from the batteries. Reduce the load. Contact Schneider Electric.
Battery disconnected The batteries are not connected. Connect the batteries.
Battery end of discharge The battery capacity is below the minimum acceptable value. Recharge the batteries.
Battery float charging The batteries are charged with the configured float charge voltage.  
Battery log reset Reset the battery log.  
Batt maint incomplete The battery maintenance test was not passed.  
Battery maintenance Battery maintenance test has started.  
Battery maintenance OK The battery maintenance test has been successfully completed.  
Battery overvoltage The battery voltage exceeds the limit. Check the battery voltage.
Battery temperature high The battery temperature is too high. Check the battery temperature.
Battery test Battery test has started.  
Battery test incomplete The battery test was not passed.  
Battery test OK The battery test has been successfully completed.  
Battery voltage low Low voltage on battery. Check the battery.
Battery wiring incorrect The battery wiring is incorrect. Check the battery wiring. Contact Schneider Electric.
Battery/charger inoperable The battery or charger is inoperable. Check the battery. Check the charger. Contact Schneider Electric.
Bypass frequency exceeds limits The bypass frequency exceeds the limit. Check the status of the bypass source. Contact Schneider Electric.
Bypass out of tolerance The bypass voltage is out of tolerance. Check the status of the bypass source. Contact Schneider Electric.
Bypass overload The load is drawing more power than the bypass source can supply. Reduce the load. Contact Schneider Electric.
Bypass overload timeout The UPS can no longer support a Bypass overload situation. Reduce the load. Contact Schneider Electric.
Bypass sequence incorrect The phase rotation on bypass is incorrect. Check the status of the bypass source. Contact Schneider Electric.
Bypass unavailable The bypass source is not available. Check the status of the bypass source. Contact Schneider Electric.
Alarm cleared Clear the alarm.  
Log cleared Clear the log.  
DC bus low voltage Low voltage on the DC bu.  
DC bus overvoltage Overvoltage on the DC bus.  
Dry input contact turns off charger The dry input contact turns off the charger.  
EPO An EPO (emergency power off) device is activated. Deactivate the EPO (emergency power off) device.
Fan inoperable The UPS has one or more inoperable fans. Check the fans. Contact Schneider Electric.
Firmware version incompatible The firmware version of the inverter is detected as incompatible with the firmware version of the rectifier. Check if the firmware version for the inverter and the rectifier is the latest. Perform a firmware update on the inverter or the rectifier.
Frequency converter mode The UPS is in frequency converter mode.  
Generator input Generator is supplying the UPS.  
Inconsistent number of parallel The configured number of parallel units does not match the actual number of units in the parallel system. Check and set the number of parallel units.
Inconsistent parallel settings The parallel settings are set incorrectly. Check for inconsistent parallel settings in Configure > Ratingand Configure > Output. Set them correctly. Contact Schneider Electric.
Inlet temperature high Air inlet temperature is too high. Check the status of the air inlet. Reduce the room temperature.
Inlet temperature sensor inoperable No inlet temperature sensor is present. Check the status of the inlet temperature sensor.
Input current unbalanced Input current is unbalanced. Check the status of the input source. Contact Schneider Electric.
Input neutral unavailable Input neutral is not available. Check the status of the input neutral. Contact Schneider Electric.
Input overcurrent timeout The UPS can no longer support an Input overcurrent situation. Check the status of the input source. Contact Schneider Electric.
Inverter high temperature Inverter temperature is too high. Check the status of the inverter. Contact Schneider Electric.
Inverter IGBT inoperable The inverter IGBT is inoperable. Check the status of the inverter IGBT. Contact Schneider Electric.
Inverter inoperable The inverter is inoperable. Check the status of the inverter. Contact Schneider Electric.
Inverter shutdown The inverter is shutting down.  
Inverter data CAN incorrect Inverter data CAN is incorrect.  
Inverter firmware incompatible The inverter firmware is incompatible with the UPS.  
Inverter firmware upgrade The inverter firmware has been upgraded.  
Inverter IO CAN incorrect Inverter IO CAN is incorrect.  
Inverter overload The inverter is overloaded. Check the status of the inverter. Contact Schneider Electric.
Inverter overload timeout The UPS can no longer support an Inverter overload situation. Check the status of the inverter. Contact Schneider Electric.
Inverter protection The UPS has turned on the inverter protection. Check the inverter voltage or current.
Load on bypass The UPS is in static bypass operation and the load is supplied by the bypass source.  
Load disconnected The load has been disconnected or the unit output disconnect device UOB is open. Check the load. Close the unit output disconnect device UOB.
Load on inverter The UPS is in inverter operation mode and the load is supplied by the UPS.  
Low battery shutdown The UPS is shutting down due to battery end of discharge Recharge the batteries and restart the UPS. If autostart mode is configured, the UPS will start automatically restart when the mains return.
Main power supply not available The main power supply is not available. Check the availability of the main power supply.
Manual boost charge The UPS is in the manual boost charge mode.  
Manually exit bypass The UPS exits the bypass operation mode manually.  
Manual float charge The UPS is in the manual float charge mode.  
Manual transfer to inverter Manual transfer to inverter operation.  
Manual transfer to bypass Manual transfer to bypass operation.  
Manual shutdown Manual shutdown.  
MBB closed latch The maintenance bypass disconnect device MBB is closed, supplying the load with unprotected power from the bypass source.  
MBB open The maintenance bypass disconnect device is open.  
Module ID duplicate The module ID has a duplicate. The module ID must be unique. Check the ID of the modules.
Nominal power out of tolerance The nominal power does not match the UPS hardware. Check the status of the input source. Contact Schneider Electric.
Outlet temperature high Air outlet temperature is too high. Check the status of the air outlet. Contact Schneider Electric.
Outlet temperature sensor inoperable No outlet temperature sensor present or the outlet temperature sensor is inoperable. Check the status of the outlet temperature sensor.
Output relay disconnected

An output relay is disconnected.

Check the status of the output relays. Contact Schneider Electric.

Output relay short-circuit

An out put relay has short-circuited.

Check the status of the relays. Contact Schneider Electric.

Output short circuit A short circuit is present on the output. Check the status of the output. Contact Schneider Electric.
Output voltage detection unsuccessful The output voltage could not be detected. Check the output voltage.
Parallel cabling incorrect The parallel cabling is incorrect. Check the status of the parallel cables. Contact Schneider Electric.
Power sharing incorrect The power sharing between the UPS units is incorrect. Please check the load sharing on the UPS units. Redistribute the load between UPS units. Contact Schneider Electric.
Prohibit transferring to inverter

Transferring to inverter operation is prohibited.

 
PWM synchronization unavailable The PWM synchronization is unavailable. Check the status of the PWM sync. Contact Schneider Electric.
Rectifier firmware upgraded The rectifier firmware has been upgraded.  
Rectifier soft start incomplete The rectifier soft start is incomplete. Check the status of the rectifier. Contact Schneider Electric.
Rectifier high temperature The rectifier temperature is too high. Check the status of the rectifier. Contact Schneider Electric.
Rectifier inoperable

The rectifier is inoperable.

Check the status of the rectifier. Contact Schneider Electric.
Rectifier overload

The rectifier is overloaded.

Check if the rectifier is overloaded. Contact Schneider Electric.
Room temperature high The room temperature is high. Reduce the room temperature.
Save settings Settings have been changed.  
SPI communication inoperable SPI communication is lost between the rectifier and the inverter. Check the SPI communication between the rectifier and the inverter.
Stop test Stop the test.  
Surge protection abnormal The SPD (surge protection device) is abnormal. Contact Schneider Electric.
Synchronization pulse unavailable Sync pulse is unavailable. The UPS is not able to synchronize. Check the sync pulse. Contact Schneider Electric.
System overload The load is drawing more power than the UPS system can supply. Reduce the load. Contact Schneider Electric.
System setting incorrect The system settings are incorrect. Check the system settings. Contact Schneider Electric.
Technical check recommended A technical check is recommended. Contact Schneider Electric.
The battery self-test conditions are not met. The battery self-test conditions are not met.  
Transfer to bypass not allowed Transferring to bypass is not allowed.  
Transfers exceed limit There have been too many transfers between operation modes in a given time period. Contact Schneider Electric.
Utility voltage exceeds limit

The detected transient input voltage input has exceeded the specified safety limit.

Adjust the main power supply voltage to the allowable range.
Warranty expired Warranty is expired. Contact Schneider Electric.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?