990-66230A-001

Configure the Air Filter Reminder

When the air filter has been replaced, reset the air filter reminder.
  1. From the main menu, tap Configuration > Reminders.
    1. Set the reminder interval in the field Duration before 1st reminder based on the installation room environment, default is 360 days.
      Under Used days you can see how many days the filter has been in use.
    2. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?