990-66230A-001

Configure the Network

The network can be configured for the integrated and the optional network management card (NMC).

  1. Configure the IPv4 settings on the page for the chosen NMC:
    1. Remove the check mark for Disable integrated NMC IPv4/Disable optional NMC IPv4 to configure the IPv4. When the check mark is present, no settings can be made and the function is disabled.
    2. Set the Address mode to Manual, DHCP, or BOOTP. For manual address mode, add the values.
    3. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?