990-66230A-001

Configure the Display Preferences

  1. From the main menu, tap Configuration > General > Display.
    1. Set the Start screen saver after (minutes). After the set minutes of no activity, the screen saver will begin on the display.
    2. Tap the - or + to set the display brightness.
    3. Set the Alarm sound to Enable or Disable. This will enable/mute all alarm sounds.
    4. Set the Touch screen sound to Enable or Disable. This will enable/mute all display sounds (excluding alarm sounds).
    5. Tap the Calibration button twice to calibrate the display.
  2. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?