990-66230A-001

Isolate a Single UPS from the Parallel System

Use this procedure to shut down one UPS in a running parallel system.

NOTE: Before initiating this procedure, ensure that the remaining UPSs can supply the load.
NOTE: The following is a generic shutdown procedure. All the disconnect devices mentioned may not be present in your specific system.
  1. On this UPS, select Control > Inverter > Inverter off. Tap OK on the confirmation screen.
  2. Open UOB for this UPS.
  3. Open SSIB for this UPS.
  4. Open BB for this UPS.
  5. Open UIB for this UPS.
  6. Open MIB (if present), BIB (if present), Ext. UOB (if present) for this UPS.

    Rear View of 10-20 kVA UPS



    Rear View of 30-40 kVA UPS

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?