990-66230A-001

Configure the UPS Input

NOTE: This configuration is mandatory for correct UPS operation.
  1. From the main menu, tap Configuration > Input.
    1. Set Rated input voltage to 220 V, 230 V or 240 V, default is 230 V.
    2. Set Rated input frequency to 50 Hz or 60 Hz, default is 50 Hz .
  2. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?