990-66230A-001

Configure the UPS Output

NOTE: This configuration is mandatory for correct UPS operation when it is powered on for the first time.
  1. From the main menu, tap Configuration > Output.
    1. Set Adjusted output voltage. The adjusted output voltage range is the rated output voltage ± 10 V, default is 230 V.
    2. Set Synchronization window. The synchronization window range is 0.5 - 5 Hz, default is 3 Hz.
  2. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?